Config Tools for i.MX v12 is offline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config Tools for i.MX v12 is offline

941件の閲覧回数
steffendoster
Contributor IV

Hi,

I want to give the "Configuration Tools for i.MX" a try. I want to create a DDR config for my custom Board with an i.MX8MP on it.

But when I start the Tools and "Create a new configuration", the Processor I need isn't there and the Tool shows the Warning: "Network is not available or offline mode is on"

Well I'm writing this with the same Computer. Im Signed in here. I have no Proxy and in "Preferences" "Work offline" isn't checked!

What's going wrong?

Is this the right Forum?

Greetings
Steffen

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

918件の閲覧回数
steffendoster
Contributor IV

Gave the Register-Programming-Aid (RPA) another try and filled out everyting marked in red (or orange).

See attached RPA.

I noticed some errors in the RPA when checking the "DDR Stress test file"-Sheet:
There are two register-values set to "TBD". No wonder its not working.

Any suggestions?

0 件の賞賛
返信

935件の閲覧回数
steffendoster
Contributor IV

I already know the RegisterProgrammingAids. They are very uncomfortable and uneasy to use.

I hoped for some better tool by NXP. And I don't get it why you make this suggestion when the DDR-Tool has "Support for i.MX 8M family devices" (original from Web-Site).

I wanted this: (from your Web-Site)

  • Support for i.MX 8M family devices
  • Configuration - Simplified UI for Device configuration
  • Advanced board configuration options
  • Generation of C code for U-boot SPL driver

But I have to use the Script-Aid with complicated Excel sheets and then have to port the resulting code to the U-Boot SPL BY HAND?????

Seriously?

 

0 件の賞賛
返信