Config Tools for i.MX generates the following files (i.MX6 ULL):
- imx6ull-board.dtsi
- iomux_config.c
- iomux_config.h
- pin_mux.c
- pin_mux.h
Can anyone provide any pointers on what should be done with these files, with U-Boot / Buildroot?
Thanks!
已解决! 转到解答。
Basically, from what I have learned so far (in case this can help someone else with the same question):
Config Tools for i.Mx in this case helps to generate pin settings (mux, pull-up/-down, etc). With the .dtsi it is not a case of copy-pasting the entire file somewhere but rather copy-pasting individual lines into your Device Tree (.dts / .dtsi) in the relevant places - you need to have some idea of what you are doing with Device Tree in order to do this. Usually you would be copy-modifying an existing Device Tree from a reference board, so should be able to figure out from there where the lines need to go.
Basically, from what I have learned so far (in case this can help someone else with the same question):
Config Tools for i.Mx in this case helps to generate pin settings (mux, pull-up/-down, etc). With the .dtsi it is not a case of copy-pasting the entire file somewhere but rather copy-pasting individual lines into your Device Tree (.dts / .dtsi) in the relevant places - you need to have some idea of what you are doing with Device Tree in order to do this. Usually you would be copy-modifying an existing Device Tree from a reference board, so should be able to figure out from there where the lines need to go.
refer to the user manual:
Tool generated board-oriented device tree (DTS) DTSI file is only a snippet and not a full device tree file content. There are just basic device tree elements, initial skeleton, and processor-specific "pinfunc.h" includes together with functional groups of fsl, pins = <...> content definitions which provide the initial IOMUXC module configuration according to the tool UI defined pin routing and functional configurations. Content itself must be manually merged together with existing Linux BSP device tree file(s) in order to apply the tool generated pins configuration
the current bsp path for uboot is
dts file is: /arch/arm/dts/
pinmux file: /include/dt-bindings/pinctrl/
kernel:
dts: /arch/arm64/boot/dts/freescale/
pin mux file:/arch/arm64/boot/dts/freescale/