ConfigTools for i.MX Version 9.0 and MCIMX6Y2CVM08AV pin assignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ConfigTools for i.MX Version 9.0 and MCIMX6Y2CVM08AV pin assignment

1,061件の閲覧回数
ban45
Contributor III

Hi,

I set the pin layout with the setting tool.

After setting UART communication TX and RX, I set CTS and RTS.

The error red did not occur when setting CTS and RTS.

Swapping RTS and CTS with the tool did not result in an error.

The RX and TX were able to communicate on the board, but the RTS and CTS signals collided.

(1) Why didn't the tool generate an error?

(2) Can I change only RTS and CTS like a tool?

(3) Does the tool consider DCE / DTE registers?

(4) Is there a register that can invalidate the DCE / DTE register?

・TOOL

Cofig Tools for i.MX6 Version 9.0

・DEVICE

MCIMX6Y2CVM08AV

 

best regard.

0 件の賞賛
返信
0 返答(返信)