Hello,
Let me know in the below image(red circle), whether R514 and R520 are used as voltage divider, when we use oscillator of 24MHz.
As mentioned in Errata sheet when using oscillator, use R514 as 1Kohm and R520 as 499 ohm.
So when 3.3V levels from oscillator(Y503) are driven, its converted to 1.1V, as required for NVCC_PLL.
When using clock (Y501), R514 should be 0Ohm and R520 should be DNP.
Please confirm.
Regards,
Surendra.
Hi Surendra
please use Table 23. XTALI and RTC_XTALI DC Parameters i.MX6UL Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
and datasheet of external oscillator. Use divider if necessary, based on voltages
provided by external oscillator.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------