Changing parameters for WiFi/BT on iMX8M Mini EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing parameters for WiFi/BT on iMX8M Mini EVK

ソリューションへジャンプ
1,058件の閲覧回数
Hrithik
Contributor III

Hi,

As per our project requirement, currently we are using iMX8MM EVK and there is a need to verify if the below mentioned code exists for both WiFi+BT(AW-CM358MA) on EVK :

  • Code to select between BT/WIFI 2.4/WIFI 5GHz mode
  • Code for Continuous wave transmission
  • Code to select different Bandwidth
  • Code for selecting different channels
  • Code for selecting different Modulation
  • Code for selecting different data rate
  • Code to change the power levels

Is there a provision to dynamically change the above parameters for testing purpose.

Thanks,
Hrithik

0 件の賞賛
返信
1 解決策
1,051件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hrithik

 

for changing parameters one can look at sect.2.8 RF test mode UM11490  Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual (public...

Linux driver capabilities can be found in  NXP Wi-Fi Driver Features and Release Notes

 

Best regards
igor

元の投稿で解決策を見る

2 返答(返信)
1,046件の閲覧回数
Hrithik
Contributor III

Thanks for the documents@igorpadykov !

 

0 件の賞賛
返信
1,052件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hrithik

 

for changing parameters one can look at sect.2.8 RF test mode UM11490  Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual (public...

Linux driver capabilities can be found in  NXP Wi-Fi Driver Features and Release Notes

 

Best regards
igor