Changing parameters for WiFi/BT on iMX8M Mini EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Changing parameters for WiFi/BT on iMX8M Mini EVK

跳至解决方案
1,060 次查看
Hrithik
Contributor III

Hi,

As per our project requirement, currently we are using iMX8MM EVK and there is a need to verify if the below mentioned code exists for both WiFi+BT(AW-CM358MA) on EVK :

  • Code to select between BT/WIFI 2.4/WIFI 5GHz mode
  • Code for Continuous wave transmission
  • Code to select different Bandwidth
  • Code for selecting different channels
  • Code for selecting different Modulation
  • Code for selecting different data rate
  • Code to change the power levels

Is there a provision to dynamically change the above parameters for testing purpose.

Thanks,
Hrithik

0 项奖励
回复
1 解答
1,053 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hrithik

 

for changing parameters one can look at sect.2.8 RF test mode UM11490  Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual (public...

Linux driver capabilities can be found in  NXP Wi-Fi Driver Features and Release Notes

 

Best regards
igor

在原帖中查看解决方案

2 回复数
1,048 次查看
Hrithik
Contributor III

Thanks for the documents@igorpadykov !

 

0 项奖励
回复
1,054 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hrithik

 

for changing parameters one can look at sect.2.8 RF test mode UM11490  Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual (public...

Linux driver capabilities can be found in  NXP Wi-Fi Driver Features and Release Notes

 

Best regards
igor