Change timing register on DDR3 for the i.mx7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change timing register on DDR3 for the i.mx7?

1,118 Views
omarlifschitz
Contributor I

Hi, 

I would like to change the timing configuration for the DDR3 controller on the I.MX7 chip.  I could not find infomation  regarding these registers.

Thanks

Omar

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

909 Views
jan_spurek
NXP Employee
NXP Employee

Hello Omar,

the descriptions of the registers can be found in the Reference manual - Chapter 9 - DDR Controller and DDR PHY sections depending on which timings you want to change. Detailed descriptions of the timing parameters can be found in the JEDEC specifications.

Best Regards,

Jan

0 Kudos
Reply

909 Views
omarlifschitz
Contributor I

Hi, Jan:

Could you provide me the reference manual? Or just send me a link to it?

I have others, like: power consumtion measurement, Hardware Development Guide, etc...but not the reference manual your pointing out.

Regards

Omar

0 Kudos
Reply

909 Views
jan_spurek
NXP Employee
NXP Employee

You can find it here.

Jan

0 Kudos
Reply

909 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omar

please use ddr init tool on

i.MX7D DRAM Register Programming Aid 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply