Can the iMX7D use 64MB LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the iMX7D use 64MB LPDDR2

Jump to solution
645 Views
hefeijiutian
Contributor I

Hello sir:

I want to use iMX7D (MCIMAX7D5EVM10SD) and 64MB (512Mbits) LPDDR2, but I know from the iMX7D manual that only 512MB to 2GB LPDDR2 density is supported. so can I use a 64MB LPDDR2 for iMX7D?

Thanks a lot!

0 Kudos
1 Solution
635 Views
igorpadykov
NXP Employee
NXP Employee

Hi hefeijiutian

 

one can check if memory parameters fit to conditions described in 

Table 9-1. DDRC feature summary :

Column size of 8-12 bits
Row size of 11-16 bits

i.MX 7Dual Applications Processor Reference Manual 

 

Best regards
igor

View solution in original post

0 Kudos
2 Replies
636 Views
igorpadykov
NXP Employee
NXP Employee

Hi hefeijiutian

 

one can check if memory parameters fit to conditions described in 

Table 9-1. DDRC feature summary :

Column size of 8-12 bits
Row size of 11-16 bits

i.MX 7Dual Applications Processor Reference Manual 

 

Best regards
igor

0 Kudos
616 Views
hefeijiutian
Contributor I

Thanks a lot sir!

0 Kudos