Can the iMX7D use 64MB LPDDR2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can the iMX7D use 64MB LPDDR2

跳至解决方案
716 次查看
hefeijiutian
Contributor I

Hello sir:

I want to use iMX7D (MCIMAX7D5EVM10SD) and 64MB (512Mbits) LPDDR2, but I know from the iMX7D manual that only 512MB to 2GB LPDDR2 density is supported. so can I use a 64MB LPDDR2 for iMX7D?

Thanks a lot!

0 项奖励
回复
1 解答
706 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hefeijiutian

 

one can check if memory parameters fit to conditions described in 

Table 9-1. DDRC feature summary :

Column size of 8-12 bits
Row size of 11-16 bits

i.MX 7Dual Applications Processor Reference Manual 

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
707 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hefeijiutian

 

one can check if memory parameters fit to conditions described in 

Table 9-1. DDRC feature summary :

Column size of 8-12 bits
Row size of 11-16 bits

i.MX 7Dual Applications Processor Reference Manual 

 

Best regards
igor

0 项奖励
回复
687 次查看
hefeijiutian
Contributor I

Thanks a lot sir!

0 项奖励
回复