Can't find IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't find IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

ソリューションへジャンプ
1,729件の閲覧回数
floriang
Contributor III

Hello,

There used to be an exe file to restore SABRE demo images on freescale website.

IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

Now I went to the website and the download link is gone!

Is there a place where I can download this file again? I need to restore an SD card to factory default!

Or could someone from freescale(or someone who downloaded the file) could attach it to this post, or post a download link as an answer?

Thank you.

Florian

タグ(2)
0 件の賞賛
返信
1 解決策
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

I will try to share the file.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
1,436件の閲覧回数
Yuri
NXP Employee
NXP Employee

I will try to share the file.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,435件の閲覧回数
richardjortega
Contributor I

I don't see this listed within the OS section of any IMX6 Page, all I can find is the IMX6SL_EVK_SDP_SD_DEMO... I cannot find anywhere the IMX6_DQ_SDP_SD_DEMO_IMAGE, can you provide a link? YuriMuhin_ng

0 件の賞賛
返信
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

The link has been sent.

0 件の賞賛
返信
1,435件の閲覧回数
arunachalamrama
Contributor III

I am also in need of the file: IMX6_DQ_SDB_SD_DEMO_IMAGE

Could some one please share the file / link?

Thanks,

Arun

0 件の賞賛
返信
1,434件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

let me know Your e-mail or please create new query :

 

1)     Please open www.nxp.com

2)     On the top level menu,

        select Support > Sales and Support (http://www.nxp.com/support/sales-and-support:SUPPORTHOME).

3)     On the bottom of the page, select Hardware & Software.

4)     Register with your business email to access the technical NXP online support.

5)     A verification email will be sent to your account. Click the embedded link to verify your access.

6)     On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process

Regards,

Yuri.

0 件の賞賛
返信
1,435件の閲覧回数
arunachalamrama
Contributor III

Hi Yuri,

I registered with my email id. Have not got the verification email even after "resend verification email".

Shall I share my email id here itself?

Regards,

Arun

0 件の賞賛
返信
1,435件の閲覧回数
arunachalamrama
Contributor III

Hi Yuri,

I submitted new query:

Case 00064748

Hope this helps.

Regards,

Arun

0 件の賞賛
返信
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

1,435件の閲覧回数
arunachalamrama
Contributor III

Thanks, Yuri, for the quick action !

This solved the problem.

Regards,

Arun

0 件の賞賛
返信