Can't find IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

Jump to solution
1,325 Views
floriang
Contributor III

Hello,

There used to be an exe file to restore SABRE demo images on freescale website.

IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe)

Now I went to the website and the download link is gone!

Is there a place where I can download this file again? I need to restore an SD card to factory default!

Or could someone from freescale(or someone who downloaded the file) could attach it to this post, or post a download link as an answer?

Thank you.

Florian

Tags (2)
0 Kudos
Reply
1 Solution
1,031 Views
Yuri
NXP Employee
NXP Employee

I will try to share the file.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
9 Replies
1,032 Views
Yuri
NXP Employee
NXP Employee

I will try to share the file.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,031 Views
richardjortega
Contributor I

I don't see this listed within the OS section of any IMX6 Page, all I can find is the IMX6SL_EVK_SDP_SD_DEMO... I cannot find anywhere the IMX6_DQ_SDP_SD_DEMO_IMAGE, can you provide a link? YuriMuhin_ng

0 Kudos
Reply
1,031 Views
Yuri
NXP Employee
NXP Employee

The link has been sent.

0 Kudos
Reply
1,031 Views
arunachalamrama
Contributor III

I am also in need of the file: IMX6_DQ_SDB_SD_DEMO_IMAGE

Could some one please share the file / link?

Thanks,

Arun

0 Kudos
Reply
1,030 Views
Yuri
NXP Employee
NXP Employee

Hello,

let me know Your e-mail or please create new query :

 

1)     Please open www.nxp.com

2)     On the top level menu,

        select Support > Sales and Support (http://www.nxp.com/support/sales-and-support:SUPPORTHOME).

3)     On the bottom of the page, select Hardware & Software.

4)     Register with your business email to access the technical NXP online support.

5)     A verification email will be sent to your account. Click the embedded link to verify your access.

6)     On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process

Regards,

Yuri.

0 Kudos
Reply
1,031 Views
arunachalamrama
Contributor III

Hi Yuri,

I registered with my email id. Have not got the verification email even after "resend verification email".

Shall I share my email id here itself?

Regards,

Arun

0 Kudos
Reply
1,031 Views
arunachalamrama
Contributor III

Hi Yuri,

I submitted new query:

Case 00064748

Hope this helps.

Regards,

Arun

0 Kudos
Reply
1,031 Views
Yuri
NXP Employee
NXP Employee

Done !

1,031 Views
arunachalamrama
Contributor III

Thanks, Yuri, for the quick action !

This solved the problem.

Regards,

Arun

0 Kudos
Reply