Can qemu emulate i.MX 8M Plus ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can qemu emulate i.MX 8M Plus ?

3,614件の閲覧回数
mm2021
Contributor III

We do not have i.MX 8M Plus board, so I'd like to ask if qemu can emulate i.MX 8M Plus?

I'd like to run qemu Linux based on i.MX 8M Plus.

Can the qemu Linux run applications compiled by XTENSA, like the SOF project?

Thank anyone who can give any information.

0 件の賞賛
返信
3 返答(返信)

3,611件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mm2021,

The qemu-system-aarch64 binary supports all the 32-bit CPUs and boards, in the same way that qemu-system-x86_64 lets you run a 32-bit x86 CPU guest, which is why the list is so long and full of 32-bit boards. You cannot just try to use a 32-bit board with a -cpu cortex-a53, since is 64 bits.

 

Regards

 

0 件の賞賛
返信

3,603件の閲覧回数
mm2021
Contributor III

Thank you for the reply.

Could  I ask for another question about qemu + i.MX 8M Plus?

I'd like to know qemu + i.MX 8M Plus supports emulating xtensa dsp core?

How to run a xtensa application under qemu + i.MX 8M Plus?

0 件の賞賛
返信

3,582件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

no, Xtensa is not supported by qemu.

 

0 件の賞賛
返信