Can imx6q android4.4.2 support 5.0Megapixel usb camera?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can imx6q android4.4.2 support 5.0Megapixel usb camera?

866 Views
conteczxy
Contributor III

Hi,

Can imx6q android4.4.2 support 5.0Megapixel usb camera?

My environment:

kernel 3.0.35

android 4.4.2

when I plug in 5.0M usb camera, the system camera app can preview, but when I click capture button, it just generate a image totally white.

However, if I tried with a 0.3M usb camera, it works well.

What is the problem? how to use 5M usb camera in my android 4.4.2 with imx6q?

Best wishes,

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

601 Views
joanxie
NXP TechSupport
NXP TechSupport

what input format and framerate do you use? IPU can support up to 240Mhz,

operating frequency of the interface is calculated in the following way:

F = FH * FW * FPS * BI * DF, BI=1.35, DF = data format, defines the number of cycles needed to send a single pixel.

0 Kudos
Reply