in reference manual, "With an addressable screen size up to 1024x480, the LCDIF provides powerful
graphics processing with low power consumption.", but it can support RK055HDMIPI4M* (MIPI 接口, 5.5",720 x 1280), so which one is correct?
Hi @WMY ,
Both are correct. In fact, resolution is not important. The key is frame rate. Too high resolution may have low frame rate because LCD_DLCK max clock is 60Mhz.
Regards,
Jing
how about MIPI interface, is it have restriction as LCD if?