Can IMX6 solox M4 transmit Ethernet data on FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can IMX6 solox M4 transmit Ethernet data on FreeRTOS

748 Views
964884547
Contributor I

For example, can the M4 core of IMX6 solox transmit data over Ethernet with external devices under FreeRTOS, and if so, where can the driver be obtained? Or should we develop it by ourselves?

Labels (1)
0 Kudos
1 Reply

670 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sinber

attached Release Notes p.2 describes what is supported in FreeRTOS for i.MX 6SoloX.

For other peripherals one will have to add support himself.

FreeRTOS for i.MX 6SoloX

https://www.nxp.com/webapp/Download?colCode=FREERTOS_MX6SX_1.0.0_WIN&appType=license 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos