Can IMX6 solox M4 transmit Ethernet data on FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can IMX6 solox M4 transmit Ethernet data on FreeRTOS

749件の閲覧回数
964884547
Contributor I

For example, can the M4 core of IMX6 solox transmit data over Ethernet with external devices under FreeRTOS, and if so, where can the driver be obtained? Or should we develop it by ourselves?

ラベル(1)
0 件の賞賛
1 返信

671件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sinber

attached Release Notes p.2 describes what is supported in FreeRTOS for i.MX 6SoloX.

For other peripherals one will have to add support himself.

FreeRTOS for i.MX 6SoloX

https://www.nxp.com/webapp/Download?colCode=FREERTOS_MX6SX_1.0.0_WIN&appType=license 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛