My CPU happens to be the i.MX6ULL.
If I write fuses, and want the fuses to take effect, I do a reset command in U-Boot.
I then want to boot U-Boot again with my new fuse settings.
If I do that, I have to start a new uuu execution because uuu exits with an error.
In the uuu.auto script I do:
FB: ucmd reset
Then I would like to do:
SDP: boot -f u-boot-image2.imx
Is there a way to tell UUU to wait for the USB bus to come up again, rather then getting an error and exiting?
Here is the output:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.43-0-ga9c099a
Success 0 Failure 1
1:12 3/ 4 [Bulk(R):LIBUSB_ERROR_PIPE ] FB: ucmd reset
After uuu exits, and the USB bus comes back, I can start uuu again and it works, but it would be nice if uuu could get past this error and continue execution when the USB bus is restored.
After issuing the acmd, I seem to be unable to issue more commands.
Here is one of many combinations I have tried:
uuu_version 1.5.65
SDP: boot -f u-boot-iotr-usb.imx
FB: ucmd echo Ready to reset
FB: acmd reset
FB: delay 10000
FB[-t 20000]: ucmd echo '****FAILS****'
FB: ucmd echo '2nd command'
FB: Done
The response I see is as follows:
Wait for Known USB Device Appear...
New USB Device Attached at 1:132-
1:132->Start Cmd:SDP: boot -f u-boot-iotr-usb.imx
100%1:132->Okay (6.185s)
New USB Device Attached at 1:132-111279D7614ECC8E
1:132-111279D7614ECC8E>Start Cmd:FB: ucmd echo Ready to reset
1:132-111279D7614ECC8E>Okay (0.002s)
1:132-111279D7614ECC8E>Start Cmd:FB: acmd reset
1:132-111279D7614ECC8E>Okay (0s)
1:132-111279D7614ECC8E>Start Cmd:FB: delay 10000
New USB Device Attached at 1:132-
1:132->Start Cmd:SDP: boot -f u-boot-iotr-usb.imx
100%1:132->Okay (6.182s)
New USB Device Attached at 1:132-111279D7614ECC8E
1:132-111279D7614ECC8E>Start Cmd:FB: ucmd echo Ready to reset
1:132-111279D7614ECC8E>Okay (0.001s)
1:132-111279D7614ECC8E>Start Cmd:FB: acmd reset
1:132-111279D7614ECC8E>Okay (0s)
1:132-111279D7614ECC8E>Start Cmd:FB: delay 10000
New USB Device Attached at 1:132-
1:132->Start Cmd:SDP: boot -f u-boot-iotr-usb.imx
100%1:132-111279D7614ECC8E>Okay (10s)
1:132-111279D7614ECC8E>Start Cmd:FB[-t 20000]: ucmd echo '****FAILS****'
1:132-111279D7614ECC8E>Fail detach kernel driver failure(0s)
Note that the reset is issued twice, even though it only occurs once in my code. I would like there to be one "reset".
I have not found a way to issue commands to U-Boot after the "acmd reset". The last message from U-Boot is "Run fastboot". The FAILS message is not printed.
"lst" does not appear in the uuu manual.
What is your intent?
Do you mean two uuu command files and two executions of uuu.exe?
Or is there some way to execute two uuu command files from the same execution of uuu.exe?