Hi All,
I am starting a project that will take input from a greyscale camera (8 bits to test on a i.MX53 QSBR and later 14 bits on a custom board using a i.MX6Solo). It is not clear to me how to set the CSI0 port up to accept greyscale data.
Table 45-2 of the i.MX53 Reference Manual Rev 2. 12/2011 states that modes for greyscale are supported for both 8 bit and 16 bit.
Looking at the CSI0_SENS_DATA_FORMAT field in the IPU_CSI0_SENS_CONF register (Section 45.51.111), it is not intuitively obvious what to select for a greyscale format:
000 full RGB or YUV444
001 YUV422
010 YUV422
011 Bayer or Generic Data
100 RGB565
101 RGB555
110 RGB444
111 JPEG
Digging even further, the data sheet has a table (Table 58 in section 4.7.8.1) shows how to connect the CSI0 pins for the respective color formats. A pure greyscale mode is not present (even though greyscale could be placed in a YUV format without the UV). The generic data mode is also not clear.
Has anyone attempted to use the greyscale mode for camera input on CSI0?
(I have a thread going with my local FAEs but I wanted to open this discussion up).
Thanks!
Any updates? I am running into the same issue with the imx6.
The way I solved this problem is I capture as RGB24 which is supported but I specify horizontal resolution as h_res/3 i.e. I fool CSI interface to think that every 3 gray pixels are one rgb pixel. You need to make sure that h_res/3 comes out divisible by 16 and v_res has to be divisible by 8. For example h_res/3=2592/3 and 1296/3 (x2 binning for 5MP gray scale camera) will work.
Thank you for the info... it may definitely help me in the future. For IMX6, I resolved it as well... see https://community.freescale.com/thread/306822
Basically, just added support for Grayscale so I did not have to change the upper (user) layer.
Good that you resolved your issue and thanks for the pointer to the native gray scale support. I'll give it a try.
Hi Brilliantov Kirill Vladimirovich,
probably I can not help you with your questions according the Linux BSP.
As you can see from the file I attached for Jim Malone (ForJim.zip), I programmed the capturing of the grayscale camera
at a very low level, register by register, with the IAR compiler for ARM. And at the end I watched the picture via a memory dump. I did not use the BSP in my code.
BR Klaus
Hi Jim,
I connected a monocrome WVGA camera to CSI0 using parallel 8 bit interface
(CSI0_DAT19-12, CSI0_PXCLK, CSI0_HSYNC, CSI0_VSYNC and I2c2).
I attached a file demonstrating my setup, which worked after a lot of
try and error because the manuals are often not very helpful.
I hope this helps.
BR Klaus