CAN-FD Support of SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN-FD Support of SoloX

Jump to solution
1,379 Views
ko-hey
Senior Contributor II

Hi all

I'm planning to use FLEXCAN module of SoloX as CAN-FD.

According to RM, it seems that the module can be used to CAN-FD.

Then, I have questions about it.

1.Can SoloX support CAN-FD ?

2.How much is maximum bit rate when I use FLEXCAN module as CAN-FD?

ko-hey

Tags (3)
0 Kudos
Reply
1 Solution
729 Views
ko-hey
Senior Contributor II

Hi Igor

You are not understand my intention.

I already checked RM but there were no description about CAN-FD.

So I posted this question.

However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.

Thank you for your cooperation.

ko-hey

View solution in original post

0 Kudos
Reply
2 Replies
729 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

FLEXCAN supported features are given in latest SoloX

IMX6SXRM sect.27.1.2 FLEXCAN Module Features

IMX6SXCEC. None mentions its support.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

730 Views
ko-hey
Senior Contributor II

Hi Igor

You are not understand my intention.

I already checked RM but there were no description about CAN-FD.

So I posted this question.

However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.

Thank you for your cooperation.

ko-hey

0 Kudos
Reply