Hi all
I'm planning to use FLEXCAN module of SoloX as CAN-FD.
According to RM, it seems that the module can be used to CAN-FD.
Then, I have questions about it.
1.Can SoloX support CAN-FD ?
2.How much is maximum bit rate when I use FLEXCAN module as CAN-FD?
ko-hey
Solved! Go to Solution.
Hi Igor
You are not understand my intention.
I already checked RM but there were no description about CAN-FD.
So I posted this question.
However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.
Thank you for your cooperation.
ko-hey
Hi ko-hey
FLEXCAN supported features are given in latest SoloX
IMX6SXRM sect.27.1.2 FLEXCAN Module Features
IMX6SXCEC. None mentions its support.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
You are not understand my intention.
I already checked RM but there were no description about CAN-FD.
So I posted this question.
However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.
Thank you for your cooperation.
ko-hey