CAN-FD Support of SoloX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN-FD Support of SoloX

跳至解决方案
1,428 次查看
ko-hey
Senior Contributor II

Hi all

I'm planning to use FLEXCAN module of SoloX as CAN-FD.

According to RM, it seems that the module can be used to CAN-FD.

Then, I have questions about it.

1.Can SoloX support CAN-FD ?

2.How much is maximum bit rate when I use FLEXCAN module as CAN-FD?

ko-hey

标记 (3)
0 项奖励
回复
1 解答
778 次查看
ko-hey
Senior Contributor II

Hi Igor

You are not understand my intention.

I already checked RM but there were no description about CAN-FD.

So I posted this question.

However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.

Thank you for your cooperation.

ko-hey

在原帖中查看解决方案

0 项奖励
回复
2 回复数
778 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

FLEXCAN supported features are given in latest SoloX

IMX6SXRM sect.27.1.2 FLEXCAN Module Features

IMX6SXCEC. None mentions its support.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

779 次查看
ko-hey
Senior Contributor II

Hi Igor

You are not understand my intention.

I already checked RM but there were no description about CAN-FD.

So I posted this question.

However, I confirmed by myself and understood that FLEXCAN module is not support CAN-FD.

Thank you for your cooperation.

ko-hey

0 项奖励
回复