Hi community,
I'm working on i.MX6 sabresd Quad platform with no pmic and using Android as my OS system.
Because of this reason, I need to build a new firmware image for my platform.
change u-boot-imx6qsabre_sd.imx
I used Yocto Project to build uboort firmware for platform.
First, I run "bitbake u-boot-mfgtool" then start to modify new uboot firmware.
But now I got several questions here.
Question:
Hi tsung
as described in sect.6.2 Manufacturing Tool, MFGTool attached Yocto
Guide, imx_v7_mfg_defconfig should be used.
If there is no pmic, it is necessary to remove all pmic references in uboot
and Linux, drivers using pmic are described in Chapter 21-24 Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------