Build mfgtool uboot firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build mfgtool uboot firmware

3,032 Views
wangtsungli
Contributor IV

Hi community,

I'm working on i.MX6 sabresd Quad platform with no pmic and using Android as my OS system.

Because of this reason, I need to build a new firmware image for my platform.

change u-boot-imx6qsabre_sd.imx

未命名.png

I used Yocto Project to build uboort firmware for platform.

First, I run "bitbake u-boot-mfgtool" then start to modify new uboot firmware.

But now I got several questions here.

Question:

  1. Which defconfig do I need to use? mx6qsabresdandroid_defconfig or mx6qsabresd_defconfig?
  2. I need to modify uboot driver for my platform (No PMIC), what should I be noticed when I designed it?
0 Kudos
Reply
1 Reply

2,477 Views
igorpadykov
NXP Employee
NXP Employee

Hi tsung

as described in sect.6.2 Manufacturing Tool, MFGTool attached Yocto

Guide, imx_v7_mfg_defconfig should be used.

If there is no pmic, it is necessary to remove all pmic references in uboot

and Linux, drivers using pmic are described in Chapter 21-24 Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply