Hi community,
I'm working on the i.MX6 sabresd Quad platform with no PMIC.
While I try to burn image with mfgtool and I received log that show no pmic detected.
So I assumed that I need to build new uboot and kernel for mfgtool.
I had set the environment for Yocto project and try to build uboot image and kernel image with "bitbake linux-imx-mfgtool" and "bitbake u-boot-mfgtool" .
But I do not know where can I modify uboot code to avoid detecting pmic.
Question:
解決済! 解決策の投稿を見る。
Using Yocto Project and bibake mfgtool-linux-imx for kernel firmware and bitbake u-boot-mfgtool for uboot firmware.
Using Yocto Project and bibake mfgtool-linux-imx for kernel firmware and bitbake u-boot-mfgtool for uboot firmware.
Does this provide me a single image wich include uboot, kernel and fs in a xxx.imx format that i could download it direktly via the imx_usb_loader?
I'm not really sure that it could do that.
But what I mentioned just can build kernel driver image and uboot image separately.
what are the contents of bitbake command files mfgtool-linux-imx.bb u-boot-mfgtool.bb?