Hi, I'm having some trouble with booting the imx8mq_evk from serial. It looks like it hangs in the restore_boot_params(); in the spl_board_init(void); function in board/freescale/imx8mq_evk/spl.c.
Have tried with both the BSP image "imx-boot-imx8mqevk-sd.bin-flash_evk" and one that is compiled from source, and two devkits with no success. Serial tools used is the imx_usb and uuu.
Does anyone have any tips?
Hi Bob
one can try with Linux Binary Demo Files - i.MX 8MQuad EVK
program it using mfg tool
Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX8MQ
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sorry, I didn't have any success with those. It looks like the image gets transferred to target correctly, but hangs when starting up. Please look at the attached picture to see console printout.
Best regards Bob Alice