Booting i.MX8MQ_EVK from serial hangs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting i.MX8MQ_EVK from serial hangs

815 Views
bob_alice_thorv
Contributor I

Hi, I'm having some trouble with booting the imx8mq_evk from serial. It looks like it hangs in the restore_boot_params(); in the spl_board_init(void); function in board/freescale/imx8mq_evk/spl.c.

 

Have tried with both the BSP image "imx-boot-imx8mqevk-sd.bin-flash_evk" and one that is compiled from source, and two devkits with no success. Serial tools used is the imx_usb and uuu.

 

Does anyone have any tips?

Labels (1)
0 Kudos
2 Replies

518 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

one can try with Linux Binary Demo Files - i.MX 8MQuad EVK

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&appType=license&location=null&Parent... 

program it using mfg tool

Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX8MQ

https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.88_2.0.0_8MQ_MFG_TOOL&appType=license&location... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

518 Views
bob_alice_thorv
Contributor I

Sorry, I didn't have any success with those. It looks like the image gets transferred to target correctly, but hangs when starting up. Please look at the attached picture to see console printout.

Best regards Bob Alice

0 Kudos