Hi
I've made a custom board using i.MX6UL G2 variant and need to boot OS form uSD card connected to uSDHC1 port.
Following are the pins can be used for card detect function-
CSI_DATA05
GPIO1_IO03
UART1_RTS_B
EVK board use UART1_RTS_B for card detect function, but as all three are in list, I've connected GPIO1_IO03 in my board and because of what I can't boot from uSD card as the CPU can't detect any card in slot because of this changed CD pin.
I've tried replacing the pin in EVK as well and it's also showing the same behavior.
Now my question is how can I shift the CD function to GPIO1_IO03 so that I can boot from sd card?
Any help is appreciated
Thanks
Punit Kumar
Solved! Go to Solution.
Hi Punit
for SD1 booting only UART1_RTS can be used according to Table 8-18. SD/MMC IOMUX Pin
Configuration i.MX6UL Reference Manual.
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
As for linux one can refer to sect.32.2.3 Devicetree Binding attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Punit
for SD1 booting only UART1_RTS can be used according to Table 8-18. SD/MMC IOMUX Pin
Configuration i.MX6UL Reference Manual.
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
As for linux one can refer to sect.32.2.3 Devicetree Binding attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor for the information.
It seems I need to make another board to get sd card work.
Regards
Punit Kumar