Booting U-boot on i.MX6 Solo X from QSPI on SABRE-SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting U-boot on i.MX6 Solo X from QSPI on SABRE-SD

1,770 Views
andrewwayner
Contributor I

Is there a documented procedure on how to modify the U-boot to allow it to be booted from QSPI flash on the SABRE-SD? All examples, including AN5127, seem to only boot U-boot from the SD-card. I would like to U-boot to be resident and boot from QSPI flash. Please advise as to how this is accomplished.

Labels (1)
0 Kudos
Reply
2 Replies

844 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Andrew,

You could also refer to the following example document:

Customizing MQX applications on i.MX6SX.

Best regards!

/Carlos

0 Kudos
Reply

844 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

please look at sect.4.4.1.5 Flashing an ARM® Cortex®-M4 image on QuadSPI

attached document and thread

How to boot imx6 SABRE SD board from qspi NOR flash using MfgTool

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply