HI,
I am booting M4 bin on the imx8m mini evk boark, my SDK version is SDK_2.5.0_EVK-MIMX8MM.
I can use the u-boot to load and excure M4 bin with the command:
ext4load mmc 0:2 0x7e0000 cmsis_ii2c_int_b2b_transfer_master.bin
bootaux 0x7e0000
My question is: how can I load and boot m4 bin in the kernel?Or dynamic install and uninstall m4 bin, like kernel module?
Hi wang
one can look at suggestions provided on
https://community.nxp.com/message/1141696?commentID=1141696#comment-1141696
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------