Boot Mode iMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Mode iMX6UL

Jump to solution
1,214 Views
srcoolz
Contributor II

Hello,

If the Fuses are set to boot from NAND and BOOT_MODE set to 00 with resistors - is it possible to change the BOOT_MODE to 01 via resistors even if the Fuses and programmed.

If yes, isn't this a security issue where in someone can change the boot mode, and boot from for eg. SD Card and read all the data from NAND. 

Is there a way to prevent changing the Boot Mode once the Fuses have been programmed?

Thank you

Regards

Santhosh

Labels (1)
0 Kudos
Reply
1 Solution
894 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs, so it

is not possible to change boot mode.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
895 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs, so it

is not possible to change boot mode.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
894 Views
srcoolz
Contributor II

Hello Igor,

Thank you for pointing me to correct section. 

Regards

Santhosh

0 Kudos
Reply