Big gap between SDMA writes on EIM bus on 6sl/Linux 4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Big gap between SDMA writes on EIM bus on 6sl/Linux 4.1

1,556 Views
jayakumar2
Contributor V

Hi,

We're using a  6sl based board with Linux 4.1. We have 32-bit EIM transactions working using individual memory read/writes. We also have SDMA from host memory to EIM target (an FPGA) partially working but we're seeing unexpected large gaps within the SDMA transfers. For example, if we transfer 64 bytes in 32-bit mode, with 66MHz EIM clock, instead of seeing 16 consecutive transfers, we see the transfer split into 1 batch of 8 writes and then a pause of about 625ns and only then the 2nd batch of remaining 8 writes.

I've attached a scope screenshot.

eim_2_transaction_pause_inbetween.jpg

I've tried changing various parameters within the EIM_GCR/CS1WCRx/etc registers. Tried tweaking burst length BL, write continuous, WC and others but the gap between the 2 sequences remains the same. That leaves the 2 suspect areas as being the SDMA test driver, or the SDMA AP2AP script which is in the sdma binary in 4.1.

My current EIM settings:

0x021B8018: 00930089 00001100 0F010000 00000000
0x021B8028: 01040400 00000000

My test dmaengine setup is:

dma_cap_zero(dma_m2m_mask);
dma_cap_set(DMA_SLAVE, dma_m2m_mask);
m2m_dma_data.dma_request = 0;
m2m_dma_data.dma_request2 = 0;
m2m_dma_data.peripheral_type = IMX_DMATYPE_MEMORY;
m2m_dma_data.priority = DMA_PRIO_HIGH;
dma_m2m_chan = dma_request_channel(dma_m2m_mask, dma_m2m_filter,
&m2m_dma_data);

dma_m2m_config.direction = DMA_MEM_TO_MEM;
dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;

dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
dma_m2m_config.src_maxburst = 64;
dma_m2m_config.dst_maxburst = 64;

dmaengine_slave_config(dma_m2m_chan, &dma_m2m_config);

dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_memcpy(dma_m2m_chan, targetaddr, rbuf, 64, 0);

I've tried varying the burst size but it has no effect. I noticed some other postings on the forum which seem to suggest problems with EIM transfers, I'm wondering if there's an underlying problem. https://community.nxp.com/thread/329143 

Also, does anyone know if there's a way to develop and add our own SDMA scripts to fix the bugs/problems with the existing FSL scripts? I tried asking FSL, and initially it seemed positive but now the request thread seems to be dead: Adding ap_2_ap_fixed into sdma rom 

Thanks!

Labels (2)
Tags (3)
3 Replies

797 Views
Poussemousse
Contributor III

Hello jayakumar2,

as far as I remember, we have solved this trouble doing nothing ! Silicium Rev 1.3 of the i.MX6S (I don't know the SL behavior) corrects the issue seen on Rev 1.1 and Rev 1.2.

Please pay attention that internal architecture (for i.MX6S/D/Q) has not been prepared for such fast transfer, even if it seems obvious. People from NXP explained me that due to internal structure and pipes to go through, the time you observe is not abnormal, and they have even been surprised that correction appears in Rev 1.3.

So you should get in touch with very specialized NXP engineer if trouble is still present with the SL die.

Let us aware,

Poussemousse.

0 Kudos

797 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at the following thread, especially to final message of

Poussemousse

How to increase speed EIM consecutive acces on iMx6S  

Regards,

Yuri.

0 Kudos

797 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

please check

SDMA transfer between EIM and memory problem 

Measure SDMA Memory To Memory Copy Performance on i.MX6Q 

https://community.nxp.com/docs/DOC-106467 

https://community.nxp.com/message/521500?commentID=521500#comment-521500 

Custom sdma scripts can be developed using NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos