Bare Metal interface access on MX7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bare Metal interface access on MX7

720件の閲覧回数
demoniacmilk
Contributor IV

Hello community,

to verify custom hardware I'd like to read/write some bytes to/from different interfaces/memory.

Beacuse I dont know anything about Linux (and the linux part for this project will be done by someone else) I would like to program these tests bare metal.

KEIL is available, what kind of emulators may I use? Any?

Are there any examples for bare metal interface access?

Is the M4 capable of accessing the DDR RAM or is this RAM access exclusive for the A7? Again, any example code?

Thanks and regards,
Lars

ラベル(2)
0 件の賞賛
返信
1 返信

595件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lars

for baremetal examples one can look on FreeRTOS

Board Support Packages (3)
FreeRTOS_iMX7D_1.0.1

i.MX 7Dual Arm Cortex-A7 Processor|NXP 

>Is the M4 capable of accessing the DDR RAM or is this RAM access

>exclusive for the A7? Again, any example code?

yes, examples can be found in FreeRTOS

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信