BSP is linux L3.14.28_1.0.0-ga
Boot setting:bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk3p1 rootwait rw video=mxcfb0:dev=ldb,if=RGB666 ldb=sin0
Through the LVDS0 output, the screen is very dark
How to adjust the brightness of the screen
Please help
thanks
解決済! 解決策の投稿を見る。
Hi haibo
The IPU backlight driver implements IPU PWM backlight control for panels. It exports a
sys control file under /sys/class/backlight/pwm-backlight.0/brightness to user space.
Please refer to attached Linux Manual sect.6.2.2 IPU Backlight Driver. Also link below
may be useful.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi haibo
The IPU backlight driver implements IPU PWM backlight control for panels. It exports a
sys control file under /sys/class/backlight/pwm-backlight.0/brightness to user space.
Please refer to attached Linux Manual sect.6.2.2 IPU Backlight Driver. Also link below
may be useful.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Can not be modified
root@imx6qsabresd:/sys/class/backlight/backlight.28# ls
actual_brightness brightness max_brightness subsystem uevent
bl_power device power type
root@imx6qsabresd:/sys/class/backlight/backlight.28# cat actual_brightness
7
root@imx6qsabresd:/sys/class/backlight/backlight.28# cat max_brightness
Harry: File=drivers/video/backlight/backlight.c: Func=max_brightness_show: Line=211 max_brightness=7
7
root@imx6qsabresd:/sys/class/backlight/backlight.28# cat brightness
Harry: File=drivers/video/backlight/backlight.c: Func=brightness_show: Line=162 max_brightness=7
7
root@imx6qsabresd:/sys/class/backlight/backlight.28# echo 128 > max_brightness
-sh: echo: write error: Input/output error
root@imx6qsabresd:/sys/class/backlight/backlight.28# echo 128 > brightness
Harry: File=drivers/video/backlight/backlight.c: Func=brightness_store: Line=178 max_brightness=1
-sh: echo: write error: Invalid argument
root@imx6qsabresd:/sys/class/backlight/backlight.28# cat > brightness
120
Harry: File=drivers/video/backlight/backlight.c: Func=brightness_store: Line=178 max_brightness=1
cat: write error: Invalid argument
root@imx6qsabresd:/sys/class/backlight/backlight.28#