BSP is linux L3.14.28_1.0.0-ga,How to adjust the brightness of the screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP is linux L3.14.28_1.0.0-ga,How to adjust the brightness of the screen

Jump to solution
1,468 Views
haibohe
Contributor II

BSP is linux L3.14.28_1.0.0-ga

Boot setting:bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk3p1 rootwait rw video=mxcfb0:dev=ldb,if=RGB666 ldb=sin0

Through the LVDS0 output, the screen is very dark

How to adjust the brightness of the screen

Please help

thanks

0 Kudos
Reply
1 Solution
1,026 Views
igorpadykov
NXP Employee
NXP Employee

Hi haibo

The IPU backlight driver implements IPU PWM backlight control for panels. It exports a

sys control file under /sys/class/backlight/pwm-backlight.0/brightness to user space.

Please refer to attached Linux Manual sect.6.2.2 IPU Backlight Driver. Also link below

may be useful.

iMX6Q display adjustment

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi haibo

The IPU backlight driver implements IPU PWM backlight control for panels. It exports a

sys control file under /sys/class/backlight/pwm-backlight.0/brightness to user space.

Please refer to attached Linux Manual sect.6.2.2 IPU Backlight Driver. Also link below

may be useful.

iMX6Q display adjustment

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,026 Views
haibohe
Contributor II

Can not be modified

root@imx6qsabresd:/sys/class/backlight/backlight.28# ls

actual_brightness  brightness  max_brightness  subsystem  uevent

bl_power           device      power           type

root@imx6qsabresd:/sys/class/backlight/backlight.28# cat actual_brightness

7

root@imx6qsabresd:/sys/class/backlight/backlight.28# cat max_brightness   

Harry: File=drivers/video/backlight/backlight.c: Func=max_brightness_show: Line=211 max_brightness=7

7

root@imx6qsabresd:/sys/class/backlight/backlight.28# cat brightness    

Harry: File=drivers/video/backlight/backlight.c: Func=brightness_show: Line=162 max_brightness=7

7

root@imx6qsabresd:/sys/class/backlight/backlight.28# echo 128 > max_brightness

-sh: echo: write error: Input/output error

root@imx6qsabresd:/sys/class/backlight/backlight.28# echo 128 > brightness

Harry: File=drivers/video/backlight/backlight.c: Func=brightness_store: Line=178 max_brightness=1

-sh: echo: write error: Invalid argument

root@imx6qsabresd:/sys/class/backlight/backlight.28# cat > brightness

120

Harry: File=drivers/video/backlight/backlight.c: Func=brightness_store: Line=178 max_brightness=1

cat: write error: Invalid argument

root@imx6qsabresd:/sys/class/backlight/backlight.28#

0 Kudos
Reply