BOOT OPTIONS ON iMX8M mini board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOOT OPTIONS ON iMX8M mini board

2,255件の閲覧回数
giacomobiancala
Contributor I

Hi,

I need a clarification about boot options on iMX8M mini processor.

I am developing a custom Board based on iMX8M mini. I have 2 BOOT options.

- eMMC (on uSDHC3). In this case NVCC_NAND = 1,8V

- uSD port (on uSDHC2). In this case NVCC_SD2 =3.3V

I also have NVCC_SD1=3,3V.

I have some doubts about BOOT_CFG[6:4] and BOOT_CFG[3:1].

BOOT_MODE referred to 1,8V and the other pins referred to 3,3V. Is it ok?

Is it correct attached table?

Thanks,

Giacomo

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

You can share your schematic on mrudang.shelat@volansystech.com. If you want you can remove the project name and customer name etc.

Regards,

Mrudang

0 件の賞賛
返信

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi,

As per our email conversation, this thread is closed.

Kindly acknowledge and assign new ticket if you have any other query.

Regards,

Mrudang  

0 件の賞賛
返信

2,007件の閲覧回数
giacomobiancala
Contributor I

Hi Mrudang,

Sorry for my late answer. Finally I have defined boot options and all seems clear. If you have a private contact I can Share electrical schematics.

Regards

Giacomo

0 件の賞賛
返信

2,007件の閲覧回数
giacomobiancala
Contributor I

Hi Mrudang,

Thank you for your answer.

I changed voltages domains.

In conclusion I have all voltage domains NVCC_xxxx at 3.3V (excepted NVCC_NAND for eMMC). 

Moreover uSDHC for SD CARD is uSDHC1 instead of uSDHC2.

Did you read my attached BOOT pinout tables?

Regards,

Giacomo

0 件の賞賛
返信

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Kindly share your schematic for CPU, eMMC, SDIO and Boot section.

This will help me to provide a complete solution of your query.

Regards,

Mrudang

0 件の賞賛
返信

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Any update?

Regards,

Mrudang

0 件の賞賛
返信

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Giacomo,

Kindly provide Boot_Mode domain pin supply voltage. It should be the same power compatible with all BOOT_MODE and JTAG and Test_MODE. 

What do you mean by other pins? Kindly provide the details.

If it is the same as a compatible supply for BOOT_MODE and NVCC_JTAG, then it is good to go ahead. 

Regards,

Mrudang

0 件の賞賛
返信

2,007件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi  Giacomo,

Any updates here?

Regards,

Mrudang

0 件の賞賛
返信