BD71847 can't power IMX8MM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BD71847 can't power IMX8MM

1,802 次查看
484999697
Contributor I

Hi,

    My design reference IMX8MM-EVK design.

    Only  “LDO1” and “LDO2” has output,and the “PMIC_ON_REQ” pin can only provide 0.6V level for BD71847,should I give an external pull-up for BD71847? 

0 项奖励
回复
6 回复数

94 次查看
Bhavesh_Bhadricha
Contributor I

@weidong_sun  @peter  did you find solution to this problem?

0 项奖励
回复

1,595 次查看
_Steph_
Contributor I

Hi !

Just wonder if you find a solution to your problem ? 
I have a custom board with same reference design and first prototype has same behaviour than yours => PMIC_ON_REQ is only 0.6V and so PMIC cannot start, as he requieres 1.44V minimum to start. 

Wanted to try some pull ups on PMIC_ON_REQ to see if it changes anything.

thanks for any reply.

0 项奖励
回复

1,676 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Peter,

There exists internal pull-up resistor on the pin PMIC_ON_REQ, See datasheet and schematic, please!

1. in datasheet

pastedImage_1.png

2. in schematic

pastedImage_2.png

So you don't need external pull-up resistor on the PIN.

BUT as a test, you can try to pull it up outside, checking if BD718847 can normally work.

3. About the issue you encountered

You can check if these several pins' level are normal.

pastedImage_4.png

Try it , please!

Have a nice day!

B.R,

Weidong

0 项奖励
回复

1,676 次查看
484999697
Contributor I

Hi Weidong,

Thank you very much for your reply. 

Only pin "WDOG_B" is not low level,and extra pull-ups on pin "PMIC_ON_REQ' are useless.

But I found there is no program on Soc,this may cause the system to only work in SNVS mode,is this the cause of insufficient drive level?

Do I need to write an additional program to the register to drive the "BD71847"?

Have a nice day!

Peter

0 项奖励
回复

1,592 次查看
imx8student
Contributor I

Hi Peter,

Did you find the explaination of this behavior ? Did you put your pull-ups for PMIC_ON_REQ on 1V8 SNVS power ?

Best Regards,

0 项奖励
回复

1,676 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Peter,

   PWRON pin must be HIGH, and PMIC_ON_REQ should also be HIGH. otherwise PMIC can't normally work.

in SNVS mode, CPU can't run any application, so you couldn't configure PMIC via I2C.

   You should try your best to find why PWRON and PMIC_ON_REQ are both LOW.

Have a nice day!

B.R,

Weidong

0 项奖励
回复