Are there IBIS models for the i.MX6 Solo Lite USB pins?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there IBIS models for the i.MX6 Solo Lite USB pins?

1,030 Views
davidlindley
Contributor I

I have designed in the i.MX6 Solo Lite in my board.  I need to run SI sims on the USB traces.  I have downloaded the IBIS file, mx6sl_416mapbga13x13_autmtv, from Freescale.  I don't think the IBIS file implements a model for the USB pins.  It looks like the models for the USB D+/D- pins are listed as "NC".  Am I reading that correct?

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

721 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

yes, you are right, not all i.MX6 ibis models have usb,

for example i.MX6SDL has

IMX6_DL_S_IBIS : i.MX 6DualLIte and i.MX 6Solo IBIS File.

Probably you can use it. In general it is sufficient

to follow usb layuout guidelines in below document

IMX6SLHDG

Hardware Development Guide for i.MX 6SoloLite - User Guide

Best regards

chip

0 Kudos
Reply