Anyone know if PF3000 and/or PF3001 can support iMX6Solo?
Seems both product webpage says iMX6Solo is the "Complementary Products".
But both datasheet only specifically mentioned 6 SL/SX/UL.
and this block diagram listed 6 Solo are supported by both PMIC.
anyway, please help clarify.
Thanks.
已解决! 转到解答。
Yes, both PF3000 and PF3001 PMICs can support the i.MX6Solo processor.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, both PF3000 and PF3001 PMICs can support the i.MX6Solo processor.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is there Linux support for the PF3000 and PF3001 when using a i.MX6Solo? If not, what would adding support entail; just DTS changes?
Can voltage scaling features be used with the i.MX6Solo?
PF3000 and PF3001 seem to be distributed pre-programmed for a particular i.MX part, but I do not see variants for the i.MX6Solo. Which variants should we look at?
In general, I'm trying to decide if using a PF3000 / PF3001 in a mobile / battery application, is better than the PF0100 part with the i.MX6Solo. Thoughts?
Thanks.