Any way to use hardware acceleration to encode/decode H.264 video stream while it supports AVTP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any way to use hardware acceleration to encode/decode H.264 video stream while it supports AVTP?

ソリューションへジャンプ
2,810件の閲覧回数
killedByBugs
Contributor III

I am trying this TSN/AVB demo (link : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791#toc... ) with an imx8qxp MEK board.

I found the following content on that webpage:

Build H.264 SW plugins

AVTPDU uses H.264 as payload for streaming, this requires H.264 encoder/decoder plugins, either software or hardware accelerations. Since we upgrade the Gstreamer and its plugins to a new version, the VPU plugins cannot be used anymore. So software H.264 plugins are required: x264 for encoder, libav for decoder.

It says that VPU plugins cannot be used anymore, but I really want to use hardware acceleration. Also, that page was posted in 2021. Does any GStreamer have plugins which can do encoding/decoding hardware acceleration while it supports AVTP now? Please let me know if there is any.

Thank you in advance.

タグ(1)
0 件の賞賛
返信
1 解決策
2,780件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @killedByBugs, 

Unfortunately, that reference it is outdated. Regarding H264 encoding and decoding you can use some options that are included on our BSP.
Please have a look on the following document at Chapter 3. Decode Examples and Chapter 4. Encode Examples:
i.MX 8 GStreamer User Guide - NXP Community

I hope this information will be helpful.

Have a great day!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,781件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @killedByBugs, 

Unfortunately, that reference it is outdated. Regarding H264 encoding and decoding you can use some options that are included on our BSP.
Please have a look on the following document at Chapter 3. Decode Examples and Chapter 4. Encode Examples:
i.MX 8 GStreamer User Guide - NXP Community

I hope this information will be helpful.

Have a great day!

0 件の賞賛
返信