I've got my SABRESD board booting through SPI-NOR on ECSPI5 (hardware modified), and
I've installed the Kernel image and ROOTFS (ext2) on the eMMC, so I can now boot independent of
both the network and the SD card. So far so good.
With this configuration in place, I was on the SABRESD's console while testing a driver
and I noticed something scary...
I tftp'd a file (script) to the board and ran it. It worked fine.
Then I reset the board and allowed it to reboot (through SPI-NOR, using eMMC for kernel & rootfs).
I log in (root) and see the script where I put it, with the correct size but when I tried to execute
it, nothing happened. Then I just tried to 'cat' the file and it acted like the file was empty; however
ls -l showed me that the file size was correct. I was able to re-download the file; however, I have
no idea why the file kinda disappeared. Not good!
So, my first question is: how resilient is the file system to arbitrary resets?
Second question: is there any data regarding the best FS choice (yaffs/jffs2/ext/etc...) to use
with eMMC?
Thanks for any thoughts,
Ed
ext2 is ok to use for short term projects, but it is not a file system that is designed for extended use on a flash device in production. UBIFS and then eventually UFS are better candidates for your long term needs. In any case, unexpected resets can cause file corruption unless a write on power failure method is employed to save data that is not committed.
There are a couple of things you can do to stop corruption from happening in a limited development environment while you are testing.
1. use the halt command on shutdown
2. use the sync command after writing small amounts of data to the media
If you are generating your file system using LTIB then the jffs2 file system is created by default and could be used without much extra effort.
You can also try the other file systems by selecting them in the ltib configuration menu
$ ./ltib -m config
Then select:
Target Image Generation -> Options -> Choose your root filesystem image type
This will bring up a list of many file systems that you can choose from for the Target image
of note are ubifs and jffs2
For managed NAND devices like eMMC you should use btrfs or ext2/3/4.
Bryan,
Thanks again, never heard of btrfs, so I'll look into that.
Meanwhile, if anyone else finds themselves on a similar quest I found this
paper from Micron which seems reasonably recent and helpful...