DDR stress test and LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR stress test and LPDDR2

Jump to solution
1,221 Views
emilmyhrman
Contributor IV

Hi,

I noticed the new ddr stress test tool 1.0.0 and I'm having trouble running it on our custom board using mx6DL and single channel LPDDR2. We have the RAM mapped to start at 0x10000000 but I suspect the tool uses 0x80000000 because the execution fails.


We're having lots of problems with the DDR calibration, so I'm not sure if it's just our configuration that is the fault.


Since we don't have any source code for the stress test tool, could you please verify that it is true that it always starts at 0x80000000 for lpddr2?



I was able to run the 0.042 version, using same ddr script by selecting to test channel 1 instead. But for 1.0.0 this is no longer an option.

Labels (2)
Tags (3)
0 Kudos
1 Solution
559 Views
emilmyhrman
Contributor IV
0 Kudos
1 Reply
560 Views
emilmyhrman
Contributor IV

This was fixed in V1.0.1 i.MX6 DDR Stress Test Tool

0 Kudos