Android7 HAL can't open iio:device1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android7 HAL can't open iio:device1

1,035 次查看
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd for my CPU and the kernel version is 4.4.8.

I'm facing the problem of HAL layer of LightSensor.cpp.

When I try to opendir("/dev/iio:device1")

And it will failed to open.

How can I fix this problem?

Do I need to give more information?

If needed please tell me what else should I give more?

Thanks in Advanced!

标签 (5)
标记 (3)
0 项奖励
回复
1 回复

894 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using our BSP? Since the kernel versions that you are using is different from the ones that we use in our BSP.

Best Regards,

Diego.

0 项奖励
回复