Hello,
I'm using custom board based on i.MX53 QSB, and Android r10.2. I'm trying to get UVC camera to work.
My camera is recognised as WebCam-HM2055
Camera is visible, when it is connected:
uvcvideo: Found UVC 1.00 device WebCam-HM2055 (058f:5608)
input: WebCam-HM2055 as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/input/input3
Also /dev/video0 is created.
Also Android application: openxc/android-webcam · GitHub
gets preview from camera, but when I try to open system application "Camera", i have exception:
I/ActivityManager( 2367): Starting: Intent { act=android.intent.action.MAIN cat=[android.intent.category.LAUNCHER] flg=0x10200000 cmp=com.android.camera/.Camera } from pid 2422
I/SurfaceFlinger( 2367): mHw->getFormat() 4
I/ActivityManager( 2367): Start proc com.android.camera for activity com.android.camera/.Camera: pid=2695 uid=10030 gids={1006, 1015}
I/WindowManager( 2367): Setting rotation to 1, animFlags=1
I/ActivityManager( 2367): Config changed: { scale=1.0 imsi=0/0 loc=en_US touch=3 keys=1/1/2 nav=1/1 orien=2 layout=34 uiMode=17 seq=4}
W/dalvikvm( 2695): Exception Ljava/lang/NullPointerException; thrown while initializing Lcom/android/camera/CameraSettings;
D/AndroidRuntime( 2695): Shutting down VM
W/dalvikvm( 2695): threadid=1: thread exiting with uncaught exception (group=0x2aac0560)
E/AndroidRuntime( 2695): FATAL EXCEPTION: main
E/AndroidRuntime( 2695): java.lang.ExceptionInInitializerError
E/AndroidRuntime( 2695): at com.android.camera.Camera.onCreate(Camera.java:891)
E/AndroidRuntime( 2695): at android.app.Instrumentation.callActivityOnCreate(Instrumentation.java:1047)
E/AndroidRuntime( 2695): at android.app.ActivityThread.performLaunchActivity(ActivityThread.java:1611)
E/AndroidRuntime( 2695): at android.app.ActivityThread.handleLaunchActivity(ActivityThread.java:1663)
E/AndroidRuntime( 2695): at android.app.ActivityThread.access$1500(ActivityThread.java:117)
E/AndroidRuntime( 2695): at android.app.ActivityThread$H.handleMessage(ActivityThread.java:931)
E/AndroidRuntime( 2695): at android.os.Handler.dispatchMessage(Handler.java:99)
E/AndroidRuntime( 2695): at android.os.Looper.loop(Looper.java:123)
E/AndroidRuntime( 2695): at android.app.ActivityThread.main(ActivityThread.java:3683)
E/AndroidRuntime( 2695): at java.lang.reflect.Method.invokeNative(Native Method)
E/AndroidRuntime( 2695): at java.lang.reflect.Method.invoke(Method.java:507)
E/AndroidRuntime( 2695): at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:839)
E/AndroidRuntime( 2695): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:597)
E/AndroidRuntime( 2695): at dalvik.system.NativeStart.main(Native Method)
E/AndroidRuntime( 2695): Caused by: java.lang.NullPointerException
E/AndroidRuntime( 2695): at com.android.camera.CameraSettings.<clinit>(CameraSettings.java:63)
E/AndroidRuntime( 2695): ... 14 more
W/ActivityManager( 2367): Force finishing activity com.android.camera/.Camera
I/WindowManager( 2367): Setting rotation to 0, animFlags=1
I/ActivityManager( 2367): Config changed: { scale=1.0 imsi=0/0 loc=en_US touch=3 keys=1/1/2 nav=1/1 orien=1 layout=34 uiMode=17 seq=5}
W/ActivityManager( 2367): Activity pause timeout for HistoryRecord{2b1c6258 com.android.camera/.Camera}
D/dalvikvm( 2367): GC_EXPLICIT freed 456K, 45% free 4072K/7303K, external 1402K/4560K, paused 58ms
W/ActivityManager( 2367): Activity destroy timeout for HistoryRecord{2b1c6258 com.android.camera/.Camera}
I would like to get this camera working in Android system, not only in openxc android webcam application
Best regards,
Toxis
已解决! 转到解答。
The freescale R10.4 BSP can be downloaded from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...
Run-time software -> Operating System Software-Board Support Packages -> IMX5X_R10_4_ANDROID_SOURCECODE
I searched the R10.4 release, and attached all "UVC" named patches here. You can check if they had been applied in your BSP.
The freescale R10.4 BSP can be downloaded from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...
Run-time software -> Operating System Software-Board Support Packages -> IMX5X_R10_4_ANDROID_SOURCECODE
I searched the R10.4 release, and attached all "UVC" named patches here. You can check if they had been applied in your BSP.