DDR3 CLK connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
10,636件の閲覧回数
tarterkit_ru
Contributor III

Hello, i want use 32bit bus DDR3.

In references with 64bits bus, used DRAM_SDCLK1 diff. signal.

In 32bit also may use DRAM_SDCLK1 or need use DRAM_SDCLK0?

ラベル(4)
0 件の賞賛
返信
1 解決策
9,861件の閲覧回数
Yuri
NXP Employee
NXP Employee

Pavel, good day !

really we can consider the DRAM_CLK0 and DRAM_CLK1 as the same clock.

But jitter should be taken into account, even when we use the same clock source,
split via buffers.   

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
9,861件の閲覧回数
tarterkit_ru
Contributor III

CS0: D0~D31 ( 2 DDR3 ICs)

        CLK1

This variant is already possible?

0 件の賞賛
返信
9,861件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Pavel,

     if you do like this, Is it convenient to control diffrential resistance of CLK1 during PCB design ?

         In order to control resistance conveniently, I recommend 2nd solution:

(2) Every 16bit uses same clock. 

CS0: D0~D15 (1 DDR3 IC)

        CLK0

CS0: D16~D31 (1 DDR3 IC)

        CLK1

CS1: D0~D15 (1 DDR3 IC)

        CLK0

CS1: D16~D31 (1 DDR3 IC)

        CLK1

Regards,

  weidong

0 件の賞賛
返信
9,861件の閲覧回数
tarterkit_ru
Contributor III

Hello Sun,

It simply question, i get 3 reply without simply answer :smileyhappy:

I don't need recommendations and comments, please just tell me DRAM_CLK0 and DRAM_CLK1 it is fully equal or have specific with CS0/1

About recommendations, see pinout imx6, CLK0 and CLK1 is morror placed, as result - in references D0-D31 connected to CLK1 and D32-D63 connected to CLK0

0 件の賞賛
返信
9,862件の閲覧回数
Yuri
NXP Employee
NXP Employee

Pavel, good day !

really we can consider the DRAM_CLK0 and DRAM_CLK1 as the same clock.

But jitter should be taken into account, even when we use the same clock source,
split via buffers.   

0 件の賞賛
返信
9,861件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Pavel,

     Please refer to Yuri's advice for you ! I agree with him, too .

Regards,

Weidong

0 件の賞賛
返信
9,857件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Pavel,

      You can refer to DDR3 connections on i.MX53_Tablet_Design for your 32bit DDR3 bus. Please see attachment.

Regards,

Weidong

0 件の賞賛
返信
9,857件の閲覧回数
tarterkit_ru
Contributor III

Hello

I'm dont understand ... why imx53 schematic ...

schematic of imx53 not have questions, because bus is 32bits

imx6 have 64bits and i can't find references schematic with 32bit and datasheet don't have any instruction about CLK0/1 selection.

0 件の賞賛
返信
9,857件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Pavel,

     I have ever confirmed the similar question with HW dept, it is no problem to use low 32bit bus of i.mx6 memory interface.

In i.MX SoC , The clock source of CLK0 & CLK1 is the same. So you can use them like this:

(1) Using same clock for reading or writing one 32 bit .

CS0: D0~D31 ( 2 DDR3 ICs)

        CLK0

CS1: D0~D31 (2 DDR3 ICs)

        CLK1
(2) Every 16bit uses same clock.

CS0: D0~D15 (1 DDR3 IC)

        CLK0

CS0: D16~D31 (1 DDR3 IC)

        CLK1

CS1: D0~D15 (1 DDR3 IC)

        CLK0

CS1: D16~D31 (1 DDR3 IC)

        CLK1

    The above mothod is for you as a reference.

Regards,

Weidong

9,857件の閲覧回数
tarterkit_ru
Contributor III

Thanks!

0 件の賞賛
返信