Hi Freescale,
Here is an issue about framebuffer rotation. Please help to investigate.
[OS]
Android JB 4.2.2 & Android KK 4.4.2
[Steps]
1. Set up two framebuffers to display in U-boot, e.g. video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:dev=lcd,1920x1080M@60,bpp=32 video=mxcfb2:off video=mxcfb3:off fbmem=28M,28M
2. Install an application which supports screen rotation, such as Antutu. Here, we take Antutu as example.
3. Execute Antutu -> Go to TEST page -> Select "Stability Test"
4. The 1st framebuffer will rotate normally from landscape to portrait mode. However, the 2nd framebuffer keeps in portrait mode.
The symptoms are different between Android JB 4.2 & KK4.4.
Operations can still be performed on JB 4.2 in portrait mode.
But screen is blocked and keeps trembling on KK 4.4 when we are moving mouse.
[Expected result]
Both the 1st & 2nd framebuffers should rotate to portrait mode.
[Additional information]
This issue does not happen on Android JB 4.3.
Best regards,
Daniel
Original Attachment has been moved to: antutu_3.2.1.apk.zip
Solved! Go to Solution.
From the RD's reply, the 2nd display should not rotate according to Google design. Android 4.3 has 2nd display rotation, and that occupies more resource and may cause incorrect rendering issue. So RD considers 2nd rotation is incorrect behavior.
FYI~
Charles, please close the DI if no more issue.
Thanks,
Yixing
For JB4.2.2, you can update the GPU libs "https://community.freescale.com/docs/DOC-102590", then it will be same as JB4.3 BSP.
Hi Freescale,
I record the symptom on both JB4.2 & KK4.4 for your references.
Please see the new attached video files.
Thanks,
Daniel