Dear All,
I have followed below link (Android 5 patch) to integrate wl1831 into Android 6 in imx6 sabresd board. When I'm testing it is working with Android 5 Mobile device. But it was not working properly with Android 6 mobiles. Some of events not receiving properly.
So can you please provide me the respective patch and firmware for Android 6.
Android 5 patch reference link:
processors.wiki.ti.com/.../WL18xx_First_Time_Getting_Started_Guide_(IMX6)
Regards,
Aravinth
Hi aravinthkumar
as Android 6 is based on L4.1.15 kernel, one can look at drivers provided
for that kernel on
WiLink8 Linux Getting Started Guide Android - Texas Instruments Wiki
or port it using
http://www.jorjin.com/upload/1484543611.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Aravinth
for kernel version: 3.14.52 please follow p.2 document
http://www.jorjin.com/upload/1484543611.pdf
Best regards
igor
You need to check with the vendor for wl1831. Because the Android is not that simple like Linux.
It including the framework code changes.The vendor for wl1831 will ask you about the detailed version of Android you are using, they will provide the SDK.