Android 10 and 11 on IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android 10 and 11 on IMX6

跳至解决方案
3,647 次查看
rahmanuh
Contributor III

Hello,

Does anyone know if there will be a support for Android 10 and 11 for IMX6?

Thank you very much.

 

Best regards,

Rahmanu

0 项奖励
1 解答
3,638 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

在原帖中查看解决方案

0 项奖励
7 回复数
3,634 次查看
vinothkumars
Senior Contributor IV

Hi @rahmanuh ,

 

It will run, But, I did not test. why I am telling this should compatible because imx6 related board files definitely will  present in source. So, we can able to select the board. 

 

 

Regards,
Vinothkumar Sekar
0 项奖励
3,613 次查看
rahmanuh
Contributor III

Hi Vinothkumar,

Thanks for your reply. Yes I think so, but I suppose it will need some configuration outside the documentation from NXP. I will try to test it to see if it can run flawlessly. My biggest concern is that I wanted to see if the WiFi driver for 88W8997 and the device itself work.

Best regards,
Rahmanu

0 项奖励
3,639 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

0 项奖励
3,481 次查看
rahmanuh
Contributor III

Hi Israel,

I am just repeating arindamroy's question.

Why is Android 10 and 11 not supporting imx6 platform?

Thanks.

/rahmanu

0 项奖励
3,462 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanuh,

 

As our EVK does not match the minimum support hardware target of the latest release we decide to not continue updating to the newer versions, of course, someone could build a custom board that matches these hardware specifications but we do not support it from our side.

 

Regards,

Israel.

0 项奖励
3,614 次查看
rahmanuh
Contributor III

Hi Israel,

Thanks for sharing the link.

Best regards,
Rahmanu

0 项奖励
3,531 次查看
arindamroy
Contributor II

Hi,

Why is Android 10 and 11 supported on imx6? Is there a technical limitation?

Thanks

0 项奖励