Android 10 and 11 on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 10 and 11 on IMX6

Jump to solution
6,590 Views
rahmanuh
Contributor III

Hello,

Does anyone know if there will be a support for Android 10 and 11 for IMX6?

Thank you very much.

 

Best regards,

Rahmanu

0 Kudos
Reply
1 Solution
6,581 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

View solution in original post

0 Kudos
Reply
7 Replies
6,577 Views
vinothkumars
Senior Contributor IV

Hi @rahmanuh ,

 

It will run, But, I did not test. why I am telling this should compatible because imx6 related board files definitely will  present in source. So, we can able to select the board. 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
6,556 Views
rahmanuh
Contributor III

Hi Vinothkumar,

Thanks for your reply. Yes I think so, but I suppose it will need some configuration outside the documentation from NXP. I will try to test it to see if it can run flawlessly. My biggest concern is that I wanted to see if the WiFi driver for 88W8997 and the device itself work.

Best regards,
Rahmanu

0 Kudos
Reply
6,582 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

0 Kudos
Reply
6,424 Views
rahmanuh
Contributor III

Hi Israel,

I am just repeating arindamroy's question.

Why is Android 10 and 11 not supporting imx6 platform?

Thanks.

/rahmanu

0 Kudos
Reply
6,405 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanuh,

 

As our EVK does not match the minimum support hardware target of the latest release we decide to not continue updating to the newer versions, of course, someone could build a custom board that matches these hardware specifications but we do not support it from our side.

 

Regards,

Israel.

0 Kudos
Reply
6,557 Views
rahmanuh
Contributor III

Hi Israel,

Thanks for sharing the link.

Best regards,
Rahmanu

0 Kudos
Reply
6,474 Views
arindamroy
Contributor II

Hi,

Why is Android 10 and 11 supported on imx6? Is there a technical limitation?

Thanks

0 Kudos
Reply