Android 10 and 11 on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 10 and 11 on IMX6

ソリューションへジャンプ
6,605件の閲覧回数
rahmanuh
Contributor III

Hello,

Does anyone know if there will be a support for Android 10 and 11 for IMX6?

Thank you very much.

 

Best regards,

Rahmanu

0 件の賞賛
返信
1 解決策
6,596件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
6,592件の閲覧回数
vinothkumars
Senior Contributor IV

Hi @rahmanuh ,

 

It will run, But, I did not test. why I am telling this should compatible because imx6 related board files definitely will  present in source. So, we can able to select the board. 

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
6,571件の閲覧回数
rahmanuh
Contributor III

Hi Vinothkumar,

Thanks for your reply. Yes I think so, but I suppose it will need some configuration outside the documentation from NXP. I will try to test it to see if it can run flawlessly. My biggest concern is that I wanted to see if the WiFi driver for 88W8997 and the device itself work.

Best regards,
Rahmanu

0 件の賞賛
返信
6,597件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanu,

 

There is not support or plans for support Andrioid 10 and 11 on the imx6, sorry for the problems that this might cause you. You can find the supported devices on the next link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Regards,

Israel.

0 件の賞賛
返信
6,439件の閲覧回数
rahmanuh
Contributor III

Hi Israel,

I am just repeating arindamroy's question.

Why is Android 10 and 11 not supporting imx6 platform?

Thanks.

/rahmanu

0 件の賞賛
返信
6,420件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi rahmanuh,

 

As our EVK does not match the minimum support hardware target of the latest release we decide to not continue updating to the newer versions, of course, someone could build a custom board that matches these hardware specifications but we do not support it from our side.

 

Regards,

Israel.

0 件の賞賛
返信
6,572件の閲覧回数
rahmanuh
Contributor III

Hi Israel,

Thanks for sharing the link.

Best regards,
Rahmanu

0 件の賞賛
返信
6,489件の閲覧回数
arindamroy
Contributor II

Hi,

Why is Android 10 and 11 supported on imx6? Is there a technical limitation?

Thanks

0 件の賞賛
返信