Hi,
I have iMX8M Mini EVK.
I did setup a Yocto toolchain for version L4.14.98_2.1.0 on my Ubuntu 18.04 LTS system.
I did successfully "bitbake imx-image-multimedia"
Then I am trying to add support for openjdk-8 or openjdk-7 or openjdk-7-jre.
But got following errors:
$ bitbake openjdk-8 -c fetch
Loading cache: 100% |############################################| Time: 0:00:00
Loaded 3575 entries from dependency cache.
ERROR: Nothing PROVIDES 'openjdk-8'
openjdk-8 was skipped: You must set MACHINE_SOCARCH_SUFFIX as MACHINE_SOCARCH_FILTER is set for this SoC.
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
$ bitbake openjdk-7 -c fetch
Parsing recipes: 100% |##########################################| Time: 0:00:18
Parsing of 2632 .bb files complete (0 cached, 2632 parsed). 3575 targets, 296 skipped, 8 masked, 0 errors.
ERROR: Nothing PROVIDES 'openjdk-7'
openjdk-7-jre PROVIDES openjdk-7 but was skipped: You must set MACHINE_SOCARCH_SUFFIX as MACHINE_SOCARCH_FILTER is set for this SoC.
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
$ bitbake openjdk-7-jre -c fetch
Parsing recipes: 100% |##########################################| Time: 0:00:18
Parsing of 2632 .bb files complete (0 cached, 2632 parsed). 3575 targets, 296 skipped, 8 masked, 0 errors.
ERROR: Nothing PROVIDES 'openjdk-7-jre'
openjdk-7-jre was skipped: You must set MACHINE_SOCARCH_SUFFIX as MACHINE_SOCARCH_FILTER is set for this SoC.
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Regards,
Prashant
已解决! 转到解答。
Hi about add the OpenJDK you can see the below threads:
Hi about add the OpenJDK you can see the below threads: